A Rainbow Village, a mountain pass, and a customer visit

Post navigation

It only took a half-hour or so of driving away from our office in Taichung before it felt like we were in the middle of the rainforest – even down to the signs warning us of killer bees!!

A Rainbow Village, a mountain pass, and a customer visit

Just past the outskirts of Taichung, close to one of our customers, we came across the “Rainbow Village.”

A Rainbow Village, a mountain pass, and a customer visit.2

Several years ago, and 87 year old veteran, known now as Rainbow Grandpa, began painting his small, abandoned village. Out of bordom, mixed with the hope of saving his village, he began painting the walls, the doors, and even the ground. After years of work, Rainbow Grandpa’s plan worked, and his little abandoned village came back to life. In cooperation with the city of Taichung, the village was named a tourist attraction, quickly becoming famous.

A Rainbow Village, a mountain pass, and a customer visit.3

From the colorful Rainbow Village, we headed into the center of Taiwan, where huge mountains separate East from West. To pass these mountains, you venture across the famous mountain roads that lead you up nearly 10,500 feet! We started up the road, and what started out as a sunny day quickly changed, facing us with high winds, heavy rain, and fog – very dangerous on a mountain pass. Our iglide bearings in the car were reliable as always. We had replaced two metal rolled bearings with our plastic plain bearings in the belt tensioner of the iglide car. The plastic bearings allowed for smooth operation of the alternator, even in environments like this!

Not surprisingly, these and the 54 other plastic bearings fared the storm just fine, and we were able to safely pass through the mountains.

A Rainbow Village, a mountain pass, and a customer visit.4

A trip up a mountain like this puts a high demand on your car. Everything needs to work well, as a small failure could have tremendous consequences in a situation like this! The belt tensioner where we installed our iglide bearings, is one component to help your car meet your demands. The tensioner provides the right amount of stress to the engine belts through a tensioner pulley. Doing this ensures other components, like the alternator or power steering, operate smoothly.

One of our customers from the area is a belt-tensioner specialist, and utilize igus products in them. The belt is located on a self-made ball bearing. The ball bearing is located on top of iglide J, which connects the bearing to the shaft. The iglide J supports the work of  the belt-tensioner, while rotating and dampening the vibration. Before the customer had used a different plastic bearing before disovering iglide, but made the switch when he found it had a better wear performance at the high-frequency motions required, and also has a lower coefficient of friction.

A Rainbow Village, a mountain pass, and a customer visit.5

I’ll update you again about the tour, we’re heading North now!

-Sascha