Taiwan to Japan!

Post navigation

The Taiwanese leg of our tour has come to an end. For two weeks, we’ve been exploring the entire island, driving more than 1,670 miles. One thing I will surely remember, apart from the beautiful landscape, is the amount of scooters on the road! They are everywhere, ruling the street. igus can help increase the lifetime of the country’s most popular mode of transportation. AEON, a well-know scooter manufacturer, relied on igus bearings in the front and rear suspension, as well as the throttle valve of their scooters.

Taiwan to Japan!

The smooth movement of the throttle valve is ensured by two iglide bearings. They can not only stand the heat of the engine without a problem, but are also light in weight and low in price, making them a perfect alternative to conventional metal bearings. iglide bearings are not new to the automotive industry; they are being installed into new cars all over the world every day! The iglide on tour car is also relying on two iglide bearings in it’s throttle valve, it’s worked perfectly now for nearly 100,000 miles, driving through heavy tropical rains in Taiwan, incredible heat through the deserts, and cold temperatures in mountain regions.

Driving through Taiwan, we saw countless rice fields. Driving along the Southern coast they begin to appear, and become larger and more abundant as you head inland – some of the fields are so huge you can hardly see where they end.

Taiwan to Japan!.2

We drove to Kaohsiung, a major port city in Southern Taiwan. There, we had a booth set up at a famous boat show being held. As the last day of the show coincided with Mother’s Day, we had a special area where you could write a postcard to your mom, which even the city’s mayor took advantage of!

Taiwan to Japan!.3 Taiwan to Japan!.4

We also paid a visit to a local kindergarten on our journey. A teacher reach and heard about the orange car traveling the world, got the children excited, and they all asked for a visit! More than 130 children between the ages of 3 and 6 were there to welcome us, and even performed some songs and dancing, and loaded up the iglide car with balloons to take back to the office!

https://youtu.be/H4A6HwHtDks

Taiwan to Japan!.5

After our travels across Taiwan, it was time to head to Tokyo!! I said my goodbyes to the car as it was loaded up, I would see it after arriving in Japan and having the proper modifications done (for example, Japanese regulations require the headlights must be moved, among other small changes.). Eventually, we received the proper permits, and were free to start exploring beautiful Japan!!

For now, we are mainly in the igus Tokyo office, putting the final preparations into effect for the tour.

I will keep you updated on our travels!

-Sascha