Down into the Japanese Islands

Post navigation

When traveling for thousands of miles like we are, it’s important to have a comfy seat! Worldwide, many manufacturers use iglide bearings to improve their seats’ performance and durability, including a customer we met with along our tour!

Down into the Japanese Islands

Many seat makers are utilizing iglide bearings for the seat height adjustment, reclining functions, crash-active headrests, and adjustment motors.  The bearings are perfect with their smooth motion. We retrofit our orange car with iglide, too. They help keep the seat adjustable without any added noise or mess.

Down into the Japanese Islands.2

Depending on the weight of the passenger, the bearings must endure high static loads. With the ability to support 100N/mm2, iglide bearings could carry even the heaviest sumo wrestler across Japan. While they are very strong, the bearings are also very lightweight, weighing in at 7x less than conventional metal bearings.

Down into the Japanese Islands.3

Japan is comprised of four large islands, including the mainland, where Tokyo and Hiroshima are located. From the mainland, we continued our tour onto the island of Kyushu, the third largest of the islands.

Kyushu is famous for its hot springs – everywhere you look you see pillars of steam coming from the ground. The number of springs is due to Japan’s unique geography. Japan is situated at the edge of 3 techtonic plates, the Pacific, Phillippine, and Eurasian plates. This not only makes Japan a great location for hot springs, but for volcanoes, earthquakes, and tsunamis.  We took our car to visit Mt. Aso, the largest active volcano in Japan.

Down into the Japanese Islands.4

The land surrounding the volcano is extremely fertile, so it becomes very green and lush. The volcano had its last eruption in 2011.

From Mt. Aso, we headed back North; driving about 500 miles straight towards the city of Nagoya. This racks in nearly 2000 miles in our Japanese tour alone!

I’ll let you know where we head from here,

Sascha