Rio de Janeiro

Post navigation

As we crossed from the Norther to the Southern Hemisphere, we also changed from summer to winter. Even so, it certainly doesn’t feel like winter here in Rio de Janeiro.

Rio de Janeiro

It’s close to 90º, and despite my SPF 50, my entire face is sunburned. Good thing the iglide bearings in the car can handle this heat better than I can – they’re still working perfectly, which isn’t surprising as they’re used so often in harsher environments than these. One of our bearings, iglide T500, can even work in long-term temperatures nearing 500º! Despite the heat, Rio de Janeiro is completely beautiful.

Rio de Janeiro.2

One of our first customer visits in Brazil was outside Rio, at a factory that manufactures equipment for Brazil and Latin-America’s biggest TV network. At their factory, they were creating a custom chairs for a TV singing competition that will sound familiar to some of our readers. The chairs use igus’ PRT slewing ring bearings to rotate around smoothly, used by the TV show’s ‘singing coaches.’ The coaches will hear the contestants sing – without being able to see them. If interested in working with that contestant, the coaches will rotate their chair around to face them (sounding like any show we have here in the US??) The PRT slewing rings from igus are used because they are almost completely silent, so they will not compromise the sound quality of the TV program, and they are also maintenance-free, so the coaches can turn to face as many potential rock-stars as they want without worry.

Rio de Janeiro.3 Rio de Janeiro.4

We also had some time to explore a bit of the city, much of which is located between mountains, including the Pao de Acucar, or Sugarloaf Mountain, which rises 1,300 feet above the harbor below.

Rio de Janeiro.5

If you aren’t feeling quite ready to climb the mountain, you can take a cable-car ride to the summit, where there is a breathtaking view of the City.

Rio de Janeiro.6

From the top of Pao de Acucar, you can also get a glimpse of the ultimate symbol of Rio de Janeiro, the statue of Christ the Redeemer, located on the peak of Corcovado Mountain.  The 130 foot statue was built to celebrate 100 years of Brazil’s independence from Portugal, celebrated in 1922.  We visited the statue around sunset. The giant amazing statue, coupled with the sky’s changing colors was a sight I don’t think I will ever forget.

Rio de Janeiro.7 Rio de Janeiro.8

As a tourist in Rio, there are 2 very obvious passions of the Brazilians. Obviously, with the World Cup happening, the first one is football. I found an amazing place to join in the football obsession, at the FIFA Fan Fest at the Copacabana!

Rio de Janeiro.9

The Copacabana is one of the world’s most famous beaches, and when Brazil’s football team is playing, the Fan Fest extends across the entire thing.

Rio de Janeiro.10

At the Fan Fest, you can also experience Brazil’s second most notable passion – Samba. Before and after the matches, and throughout the night in the city, you can hear Samba music everywhere. They even have Samba schools throughout the city!

We also came across a Brazilian favela. These neighborhoods are notorious for crime and corruption – until recently many were governed by gangs and criminals instead of Brazilian government. Over the past few years, gangs are starting to be expelled from the area, and local police stations are being built.

Rio de Janeiro.11

Despite its problems, Rio is a city with many facets, and surely one of the most beautiful cities worldwide.

Soon, we will leave Rio and head South until we reach the Argentinian border.

Rio de Janeiro.12

Until then,

Sascha