Seattle, WA and Portland, OR

Post navigation

We left Vancouver and headed back to the US for our next destination, Seattle, Washington. Seattle is the largest city in the Pacific Northwest region of North America and the fastest-growing major city in the United States. This city is full of character with it’s vibrant city-center and is home to Pike’s Place Market, the Space Needle, fresh, locally-sourced raw oysters, and a Ferris wheel at Pier 57.

Pike’s Place Market is an open market with everything from seafood to fresh fruit to dried flowers. The market opened in 1907 and is one of the oldest continually operating public farmer’s markets in the country. Thousands of tourists swarm the market daily to purchase fresh food and goods, steps away from one of the country’s most iconic coffee shop.

The iglide® car in front of the famous wall of gum in down town Seattle

Seattle, WA and Portland, OR

Before leaving Seattle and heading off the Portland, the car was brought to the celebrated Space Needle. The Space Needle is a landmark of the Pacific Northwest and a staple of the Seattle skyline.

Seattle, WA and Portland, OR.2

There is an observation deck from which to view the whole city of Seattle. Just like the Eiffel Tower, it was built for a world’s fair in 1962. When it first opened, nearly 20,000 people a day were taking elevators to get to the top to see the entire Seattle metropolis.

We were able to visit a fitness machinery design company that integrated our bearings in their top of the line equipment. We were able to tour their test room and see the bearings used first hand. iglide® bearings can significantly reduce noise and maintenance in fitness equipment. Their low-friction, self-lubricating operation keeps operation quiet, and eliminates the mess of oil leaking onto the machines.  Smooth operation of the iglide plastics makes machines move smoothly, making customer workouts their best.  Because they do not require external lubrication, maintenance is also unnecessary.

Our bearings inside this piece of fitness equipment 

iglide L280® bearings are a great solution for exercise equipment, possessing a low coefficient of friction, and high wear resistance. It’s also ideal for use with rough shafts or in abrasive environments, so manufacturers can use less expensive shafts in their equipment as well.

Seattle, WA and Portland, OR.4 Seattle, WA and Portland, OR.5 Seattle, WA and Portland, OR.6The car set up in the parking lot for a visit

After leaving Seattle it was time to head to Portland. Portland is a very unique city, famous for their food carts which celebrate food from almost every ethnicity you could imagine. The carts line over two blocks of the city and made picking what to eat for lunch very difficult. Some of us chose coffee from one cart, a salad from another, and desert from a third just to sample the incredible and unparalleled variety of food.

Seattle, WA and Portland, OR.7Food trucks lining the streets in Portland

Next we visited Powell’s Books, a bookstore chain located in Portland. We headed to the headquarters, dubbed Powell’s City of Books, which claims to be the largest independent new and used bookstore in the world. Besides boasting multiple buildings, inside the store each section has a color to indicate what genre the room is, because otherwise finding a book would be close to impossible.

Seattle, WA and Portland, OR.8The car going over the Hawthorne Bridge, the most well known of the multiple bridges in Portland

Our next stop is San Francisco where the car will get to drive over the Golden Gate Bridge.

We will keep you posted,

Sascha and Kayla