Minneapolis, Minnesota

Post navigation

Minnesota is known for its cheese curds, farmland, and distinct accents. The state of Minnesota is also home to the largest mall and state fair in the USA. The iglide car was fortunate enough to get to participate in all of these Minnesotan activities.

Minenapolis and St. Paul are the “Twin Cities” of Minnesota.” Minneapolis is the larger of the two, and lies between banks of the Mississippi River. The smaller of the twins, St. Paul, is the state’s capital city.

Minneapolis is abundantly rich in water, with 20 lakes, the Mighty Mississippi, and a number of creeks, waterfalls, and wetlands. It was once the word’s flour million capital and a hub for timer. Today, the city is primarily a business center between Seattle and Chicago. For being rated the country’s 14th largest metropolitan area, the city is very quiet and still. Traffic is minimal, and most restaurants are emptied by 9 PM.

In Minneapolis, we visited a number of customers, including a manufacturer of commercial and residential lawn mowers. They use iglide bearings in a variety of applications on their mowers, and choose iglide because of their ability to stand up to flying dirty, soil, and other debris that could clog and seize traditional ball bearings.

iglide plastic bearings are also able to stand up to fertilizers and other chemicals that is unavoidable in the agriculture industry. Some iglide materials, like iglide T500, can even stand up to hydrochloric acid! Good luck trying that with a standard plastic material!

Minneapolis, Minnesota

Another customer visit was to an engineering firm that works in many different industries, including wind turbines. Because of their light weight and green properties, iglide bearings are a natural fit inside. Because they are up to 8 times lighter than metal bearings, iglide bearings can reduce the weight and drive requirements of applications, and they also require less oil power to create than comparable steel bearings.

After visits to customers, the iglide car took off for the Minnesota State Fair. This year, the fair set a record for their highest attendance ever – with 252,092 people walking through the gates with 2 days to go!!

Everyone had a great time at the fair, especially those hungry people that wandered in! You could buy any type of food imaginable on a stick- from beef jerky to alligator, even a salad on a stick!

Strolling through the fair, a lumberjack show and carving contest drew quite the crowd, the competitors even had a race up and down the tree trunks using their rope skills for support.

Minneapolis, Minnesota.2 Minneapolis, Minnesota.3

From the State Fair, the car headed out for some shopping at the Mall of America – 4.3 miles of store front, or 7 Yankee Stadiums of shopping under one roof! Inside, there is even an amusement park with a fully looping roller coaster.

Minneapolis, Minnesota.4 Minneapolis, Minnesota.5

From Minneapolis, iglide on tour heads south to Iowa, Look for us on the road!

Thanks for reading,

Kayla