Let’s go back a few days to review iglide on tour’s travels from Washington DC to Niagara Falls, some of the most photographed areas of the United States!
After more than 2 months on the road across North America, iglide on tour finally made it to the United State’s capital, Washington DC. DC, short for District of Columbia, is a 68 square mile area between Maryland and Virginia that serves as the capital city of the United States. The city is a perfect representation of the US’s “Melting Pot” nature; the city is home to more than 170 embassies and international cultural centers. Local colleges and universities host about 20,000 international students each year, and 15% of DC residents speak a language other than English at home. All that diversity surrounds countless memorials, statues, and icons that represent American history and heritage.
While in DC, the iglide car visited the Lincoln Memorial, Washington Monument, and the White House, likely the three most famous landmarks in the country. The Lincoln Memorial, seen above, is a monument dedicated to the US’ 16th President, Abraham Lincoln. Showcasing a seated Lincoln, surrounded by engravings of two well-known speeches by Lincoln, The Gettysburg Address, and his second Inaugural Address, the memorial has been the site of many famous speeches, including Martin Luther King’s “I Have a Dream” speech.
The Washington Monument was built to commemorate George Washington, the first President of the United States of America. The monument, which is made of marble and granite and stands a massive 555 feet tall, is the world’s largest stone obelisk.
The next stop in the nation’s capital was the White House – where the President of the United States lives while in office since 1800. Many Presidents throughout the country’s history have put their own mark on the White House, including Thomas Jefferson’s expansion of the house, Theodore Roosevelt’s relocation of the offices to the famous West Wing, and the rebuilding after the British burned much of the building during the War of 1812.
Heading North out of Washington DC, iglide on tour traveled to another city filled with US history, Philadelphia – home to the Liberty Bell, Independence Hall, and more modern landmarks like the Philadelphia Museum of Art, Reading Terminal, and a statue of famed movie boxer Rocky Balboa.
The Liberty Bell is an iconic symbol of American Independence. Commissioned in 1752, the bell is inscribed with the words “Proclaim LIBERTY throughout all the land unto all the inhabitants thereof.” The Bell, which was originally used to alert lawmakers of legislative sessions and to notify the public about meetings and proclamations. The bell cracked when it was rung for the first time, and despite multiple repairs, the crack remains.
Independence Hall, where the Liberty Bell was originally housed, is the site where America’s founding fathers gathered to sign the Declaration of Independence in 1776, the document announcing that the thirteen American colonies, then at war with Great Britain, regarded themselves as thirteen newly independent sovereign states, and no longer a part of the British Empire. 11 years later, representatives from those states came together to create the US Constitution.
There is more than just history in Philadelphia, however. One of the most famous American sports films, Rocky, notably took place in Philly, using the steps of the Philadelphia Museum of Art as a training area. A statue of Rocky, a fictional boxing legend, has been added to the bottom of the iconic 72 stone steps.
On it’s way out of Philadelphia, the iglide car made a stop at another customer, this time, Pride Mobility, a leader in the design and manufacture of mobility products, including power lift chairs and mobility scooters. Pride uses iglide bearings in a variety of their mobility products like wheelchairs. Because they are extremely wear-resistant and require no maintenance, iglide plastic bearings are an excellent solution for products that need to be used long-term, day after day, like wheelchairs and other personal mobility products. In the lift and tilt mechanisms of their wheelchairs, Pride uses igus’ iglide G300 bearings, and also uses DryLin J linear bearings to help tilt the seat. In addition to being a long-lasting solution, igus plastic components are also immune against water, dirt, and other outside elements that can affect typical ball bearings. By using components that are strong against the outside elements, Pride Mobility customers can trek out into the wild without worrying about bearing failure!
From Philadelphia, the car continued on until it reached Niagara Falls, one of North America’s most beautiful landmarks, also marking iglide on tour’s 3rd passage over the Canadian border. Made up of three waterfalls on the Niagara River, The falls are split between New York (USA) and Ontario (Canada), and include the Horseshoe Falls, which is the most powerful waterfall in all of North America.
While at the falls, the iglide bearings got the chance to go by boat around and behind the falls, getting drenched in water. Unlike metal, there was no chance of rust from the waterfall!
From Niagara, it was time for iglide on tour to head East towards New England, the final stretch of the iglide tour across North America!
Look for us on the road!
Kayla