iglide on Tour Comes to an end at the Hannover Fair

Post navigation

After 62,283 miles (100,240 km), four continents, over 30 countries and 14 months of travel, iglide on Tour has come to an end.

Just to recap the tour, the car was equipped with 56 of our bearings in a range of different applications including; the convertible top, throttle valve, alternator, window regulator, windshield wiper, handbrake, brake pedal, gear shift and seat adjustment.

The car ended its tour on display at the Hannover (Messe) Fair in Hannover, Germany. Hannover Messe is the world’s biggest industrial fair. Typically there are around 6,500 exhibitors and 250,000 visitors.

As promised, the applications were removed from the car on stage at Hannover and presented to the audience.

The results were as expected; none of the 56 assembled bearings had a trace of wear or tear.

The individual bearings weren’t dismantled from their individual components because of the danger of damaging them, but they were examined by igus experts and they all were working properly.

The car received high attention at the fair. 44 top journalists from engineering and automation media joined the press conference about the tour. People were even seen taking selfies with the car.

The car has traveled through extreme conditions while on tour; deserts and potholes in India, dirt and mud highways of Alaska, 80% humidity in Iowa, winter in the Netherlands and the congested streets of some of the biggest cities in the world (NYC, Chicago, Shanghai, Rio de Janeiro and Beijing.) It traveled by boat, by plane and even via helicopter to make it to all of its destinations. This tour truly put the bearings to the test.  Our bearings were able to withstand all of these different environments to prove that plastic bushings are not only equal, but better than metal.

The iglide car has been re-retrofitted with new bearings and is free to be used to make local customer visits in Germany.

Maybe the car will come back to the U.S. for another visit?

Stay tuned!