The Motion plastics tour in Mexico comes to an end and the last stop is in Ciudad Juarez Chihuahua

Post navigation

The Motion plastics tour in Mexico comes to an end and the last stop is in Ciudad Juarez Chihuahua. We are in the Monument to the “Mexicanidity” that is a monumental sculpture in Ciudad Juarez, Chihuahua, Mexico. It is popularly called the X or X Sebastian, both for its unusual sculptural form and  in honor to its author. The colossal monument is located in the Plaza de la Mexicanidad, which bears the same name as the sculpture, and it is located in the north of the city, right on the border with El Paso, Texas and a few meters from the Rio Bravo. The tour has left behind several dozens of people with knowledge of a wide range of products that could help them to get the cost down ..life up effect !.