Taiwan to Japan!

The Taiwanese leg of our tour has come to an end. For two weeks, we’ve been exploring the entire island, driving more than 1,670 miles. One thing I will surely remember, apart from the beautiful landscape, is the amount of scooters on the road! They are everywhere, ruling the street. igus can help increase the lifetime of the country’s most popular mode of transportation. AEON, a well-know scooter manufacturer, relied on igus bearings in the front and rear suspension, as well as the throttle valve of their scooters.

Taiwan to Japan!

The smooth movement of the throttle valve is ensured by two iglide bearings. They can not only stand the heat of the engine without a problem, but are also light in weight and low in price, making them a perfect alternative to conventional metal bearings. iglide bearings are not new to the automotive industry; they are being installed into new cars all over the world every day! The iglide on tour car is also relying on two iglide bearings in it’s throttle valve, it’s worked perfectly now for nearly 100,000 miles, driving through heavy tropical rains in Taiwan, incredible heat through the deserts, and cold temperatures in mountain regions.

Driving through Taiwan, we saw countless rice fields. Driving along the Southern coast they begin to appear, and become larger and more abundant as you head inland – some of the fields are so huge you can hardly see where they end.

Taiwan to Japan!.2

We drove to Kaohsiung, a major port city in Southern Taiwan. There, we had a booth set up at a famous boat show being held. As the last day of the show coincided with Mother’s Day, we had a special area where you could write a postcard to your mom, which even the city’s mayor took advantage of!

Taiwan to Japan!.3 Taiwan to Japan!.4

We also paid a visit to a local kindergarten on our journey. A teacher reach and heard about the orange car traveling the world, got the children excited, and they all asked for a visit! More than 130 children between the ages of 3 and 6 were there to welcome us, and even performed some songs and dancing, and loaded up the iglide car with balloons to take back to the office!

https://youtu.be/H4A6HwHtDks

Taiwan to Japan!.5

After our travels across Taiwan, it was time to head to Tokyo!! I said my goodbyes to the car as it was loaded up, I would see it after arriving in Japan and having the proper modifications done (for example, Japanese regulations require the headlights must be moved, among other small changes.). Eventually, we received the proper permits, and were free to start exploring beautiful Japan!!

For now, we are mainly in the igus Tokyo office, putting the final preparations into effect for the tour.

I will keep you updated on our travels!

-Sascha

A Rainbow Village, a mountain pass, and a customer visit

It only took a half-hour or so of driving away from our office in Taichung before it felt like we were in the middle of the rainforest – even down to the signs warning us of killer bees!!

A Rainbow Village, a mountain pass, and a customer visit

Just past the outskirts of Taichung, close to one of our customers, we came across the “Rainbow Village.”

A Rainbow Village, a mountain pass, and a customer visit.2

Several years ago, and 87 year old veteran, known now as Rainbow Grandpa, began painting his small, abandoned village. Out of bordom, mixed with the hope of saving his village, he began painting the walls, the doors, and even the ground. After years of work, Rainbow Grandpa’s plan worked, and his little abandoned village came back to life. In cooperation with the city of Taichung, the village was named a tourist attraction, quickly becoming famous.

A Rainbow Village, a mountain pass, and a customer visit.3

From the colorful Rainbow Village, we headed into the center of Taiwan, where huge mountains separate East from West. To pass these mountains, you venture across the famous mountain roads that lead you up nearly 10,500 feet! We started up the road, and what started out as a sunny day quickly changed, facing us with high winds, heavy rain, and fog – very dangerous on a mountain pass. Our iglide bearings in the car were reliable as always. We had replaced two metal rolled bearings with our plastic plain bearings in the belt tensioner of the iglide car. The plastic bearings allowed for smooth operation of the alternator, even in environments like this!

Not surprisingly, these and the 54 other plastic bearings fared the storm just fine, and we were able to safely pass through the mountains.

A Rainbow Village, a mountain pass, and a customer visit.4

A trip up a mountain like this puts a high demand on your car. Everything needs to work well, as a small failure could have tremendous consequences in a situation like this! The belt tensioner where we installed our iglide bearings, is one component to help your car meet your demands. The tensioner provides the right amount of stress to the engine belts through a tensioner pulley. Doing this ensures other components, like the alternator or power steering, operate smoothly.

One of our customers from the area is a belt-tensioner specialist, and utilize igus products in them. The belt is located on a self-made ball bearing. The ball bearing is located on top of iglide J, which connects the bearing to the shaft. The iglide J supports the work of  the belt-tensioner, while rotating and dampening the vibration. Before the customer had used a different plastic bearing before disovering iglide, but made the switch when he found it had a better wear performance at the high-frequency motions required, and also has a lower coefficient of friction.

A Rainbow Village, a mountain pass, and a customer visit.5

I’ll update you again about the tour, we’re heading North now!

-Sascha

Welcome to Taiwan!

The iglide car has arrived in Taiwan!

Our first stop in the country is Taichung City, in the Western part of the country. Taichung is also the home to our Taiwanese office, where the car and I received a warm welcome. It felt good as always to be reunited with the iglide car; after spending so much time together over the past months I’ve grown attached!

The first day in Taiwan, we were stuck waiting for driving permits for the country, but still managed to explore a bit and have some fun – someone managed to get our dry-tech box away from us and add it as a prize in an arcade machine!

After a day of waiting, we received all the proper permits for the car – the tour can officially begin!