Rocking and rolling through Cleveland

Let’s look back a few days at iglide on tour’s journey through Cleveland, Ohio – the home of Rock and Roll!

The iglide car arrived in Cleveland, home to the Rock and Roll Hall of Fame. The city originally blossomed into a commercial hub in the mid 1800’s, due to it’s location, right on the southern shore of Lake Erie, as well as its connection to multiple canals and railroad lines. The city is now home to a wide range of commercial industries, including manufacturing, financial services, healthcare, and biomedical research and development. There is also a large population of industrial publications that are headquartered in Cleveland – and it just so happens, many of them were looking forward to meeting the iglide car in person!

Rocking and rolling through Cleveland

igus is very lucky to have such a wonderful media base to meet with while in Cleveland. The car made stops at two media companies while in town, Penton and WTWH – both hoping that iglide on tour would make its way into their city.  The iglide car’s first media stop was to Penton Media, who publish magazines like Machine Design and Hydraulics & Pneumatics. The car was parked on the roof of the building’s garage – but not for long! Editors and staff had a fantastic time taking the little car for a spin – literally! While the car has had many guest drivers across North America, it has never moved as quickly as it did with excited members of the press behind the wheel! As Penton’s staff took turns whipping the little car around the garage, everyone else had a wonderful time talking about the adventure so far, and where iglide on tour is heading next. One editor, who was visiting from New York City, even planned to meet with the car in Times Square when the car arrives. After a few hours of fun, it was time to say goodbye, and head to the next visit.

Rocking and rolling through Cleveland.2Staff from Penton Media posing with the iglide car and their igus beachballs!

The second iglide on tour press visit took us across downtown Cleveland to WTWH Media, which stands for “Willing to Work Harder.” They are most well known for publishing Design World magazine, among a number of others. This visit gave the iglide car a bit of a big head, as it was like a celebrity for a few hours. Hundreds of twitter posts erupted, all thrilled with the bright orange visitor in the parking lot. The staff of WTWH shot movies, took photos, and drove the car around the large open parking area – everyone seemed to be having a fantastic time. One employee exclaimed “We have been waiting to meet this car since we found out about it eight months ago!”  Now that’s a loyal fan!


At a towering 6’9″, one of WTWH’s editors became the iglide car’s tallest passenger to date! 

During the visit, a familiar friend appeared as the staff of WTWH began filming the car. Their videographer started shooting with a DryLin camera slider, made by igus! The sliders are very popular with photographers and videographers for its very smooth and quiet sliding motion. The DryLin slider systems offer perfectly balanced friction, for the perfect sliding feel, quiet operation by using plastic liners which dampen vibrations, and requires zero external lubrication. A unique 8 bolt design prevents misalignment of the camera slider, keeping shots looking their best, and the system is also completely modular, so adding on extras is simple.

The videographer explained that he find the slider, which he got from igus at a trade show, comes in handy when shooting. “I use this slide all the time! It’s so smooth, and it helps me get the best shots that aren’t choppy or bumpy.”

Rocking and rolling through Cleveland.4A DryLin camera slider, helping to shoot the iglide car! 

Check out the video they shot using the slider, featuring an interview with our iglide Product Manger, Nicole Lang.

https://youtu.be/t9ixDFuyMGI?list=UU_FOwetQ9swJOgSeIYpXbkA

While in Cleveland, the iglide car had to stop at the Rock and Roll Hall of Fame, which is dedicated to archiving the history of the most influential artists, producers, engineers, and others in the music industry. Inside the museum, there are hundreds of iconic pieces of rock and roll memorabilia, including John Lennon’s jacket, Kurt Cobain’s guitar, and collections of items from some of the biggest music festivals in history. One of the newest exhibits features some of Beyonce’s clothes, including her performance costume from the 2013 Superbowl and the “Single Ladies” music video.

Rocking and rolling through Cleveland.5Outside the Rock and Roll Hall of Fame in Cleveland

Driving outside the city, the car decided to visit another all-american hall of fame – this one dedicated to football. American football that is! Located in Canton, Ohio, where the National Football League was originally founded, The Pro Football Hall of Fame is different from many other professional sports halls, because it does not induct officials into the hall of fame.

Rocking and rolling through Cleveland.6Outside of the Pro Football Hall of Fame

iglide on tour also made a few customer visits while in the Cleveland area, to customers specializing in very different industries, food packaging, and agricultural equipment.

Although these customers work to create very different products, they both choose igus for surprisingly similar reasons. In the food industry, cleanliness is of extreme importance. Threore, having grease or oil in a food production plant is a big “no-no.” Likewise, in a constantly dirty and dusty world of agriculture, having grease and oil can attract this dirt into bearing systems, causing them to fail. igus’ dry-tech plain and linear bearings are all completely self-lubricating, so there is no grease to spoil food, and no extra attractants for dust out in the field. During these visits, iglide on tour was able to see firsthand some of the customer applications where igus parts are being used. See if you can spot the igus parts in these photos!

Rocking and rolling through Cleveland.7A black and yellow igubal spherical bearing helps keep this application running smoothly

Rocking and rolling through Cleveland.8DryLin W linear slides help move these systems back and forth, dirt and grease free. 

Rocking and rolling through Cleveland.9These lead screw driven linear systems help label food products, while keeping everything sanitary and safe

It’s truly amazing the range of customers that iglide on tour has had the privilege of visiting over the past several months!

Check back to see what adventures iglide on tour had next!

Look for us on the road,

Kayla

San Francisco and Los Angeles

Before arriving in San Francisco, we stopped at Muir Woods Park to see the famous California Redwood Trees, just north of the city. The trees seem as tall as skyscrapers, and their trunks have such an enormous width that four people can pose for pictures inside some of the hollowed out trunks.

San Francisco and Los Angeles

While attempting to get the dry-tech box posed in front of the towering trees, it tipped over and fell off a bridge into a creek. But fear not, the dry-tech box survived the fall and the water, as the bearings are sturdy and waterproof. Sascha came to the rescue, jumping over the railing, and climbing down the bank to fish out the box.

San Francisco and Los Angeles.2

From Muir Woods we approached San Francisco. The car drove over the famous 1.7 mile-long Golden Gate Bridge into the hazy city. As we drove, the iconic fog began to roll in and cover the arches of the bridge.

San Francisco and Los Angeles.3 San Francisco and Los Angeles.4

After touring the city the iglide car had two customer visits, the first was in San Jose to a company which specializes in designing and manufacturing medical laboratory equipment. Next it was time to head to Santa Clara, where the car visited a potential customer that designs specialty bicycles, which hopes to reduce the weight of their bicycles, in addition to other advantages igus bearings can provide.

In San Francisco, the car had no problem scaling the steep (vertical) streets, reaching the top for panoramic views of the Golden Gate Bridge, and the storied Alcatraz Prison, and then driving down the well-known zigzagging Lombard Street. The hand-break was constantly in use, essential on the streets of San Francisco, putting igus bearings to the test. We were able to ride on the cable cars, which are a form of public transportation in the city, racing up and down the hills, as cars dodge the fast-moving trolleys, and passengers hang off the side of the cable cars. The car also visited Pier 39, Fisherman’s Wharf, and the Ghirardelli Chocolate Factory for a little treat.

San Francisco and Los Angeles.5Lombard Street

San Francisco and Los Angeles.6Alcatraz

San Francisco and Los Angeles.7

San Francisco has a retro feel, teaming with tourists, hipsters, and eclectic personalities. The Dungeness crabs, mussels, and fish and chips were delicious and fresh, fished from the San Francisco Bay, which hosts America’s Cup sailboat race, and is known for its vicious currents. We said goodbye to the cool mist of San Francisco and drove south to Los Angeles. We drove along the Pacific Coast Highway, stopping at Pismo Beach and Santa Barbara. From there we headed to our destination of Los Angeles.

San Francisco and Los Angeles.8

We had two customer visits in the Los Angeles area, the first with an electric car designer and manufacturer, known for their innovative and sleek style. The engineers at this beautiful design facility where highly intrigued by the iglide car, and the parts we had on display. Our next visit was to a company which provides measurement solutions designed to improve product quality and productivity for many different kinds of manufacturing equipment. One manager said if she had to sum up igus in one word she would use “excellent”, noting the reliability of the iglide line.

San Francisco and Los Angeles.9 San Francisco and Los Angeles.10 San Francisco and Los Angeles.11The iglide car was a huge hit at our customers’… Everyone was clamoring to get inside and have their photo taken! 

After the customer visits it was time to take the car on an adventure through downtown Los Angeles. After battling the infamous 405 traffic, weaving through all six lanes on the highway, the iglide car wanted to partake in the excitement of the Walk of Fame. The car posed with the Hollywood sign, made an appearance at the Beverly Hills Hotel, Sunset Boulevard, Rodeo Drive, and even spotted a celebrity or two.

San Francisco and Los Angeles.12The car with the Hollywood sign in the distance. 

San Francisco and Los Angeles.13

We are now hitting the road to Las Vegas; look for us on the strip!

Thanks for reading,

Kayla