The iglide car crosses the border! Michigan to Ontario, Canada

Let’s look back a few days as iglide on tour took on the USA/Canadian border yet again!

After leaving Chicago, the iglide car racked up a few more miles and headed to Kalamazoo, Michigan, marking the 10,000th North American mile of the tour. The car started in Anchorage, Alaska with 25,000 miles on it, and has reached 35,000 in just six short weeks! Time flies when you are driving the iglide car across the country!

The iglide car crosses the border! Michigan to Ontario, CanadaThe iglide car on the first day of the North American tour in Alaska. Little did the car know that it would have racked up 10,000 more miles six weeks later.

In Michigan, the car made a large number of customer visits to an incredibly wide range of companies. The iglide car met customers that use igus products in medical beds, amazing welded assembly systems, and, being in Michigan, a number of automotive applications!

While iglide bearings are used in a number of applications inside the iglide car, and millions of other automobiles manufactured each year, a number of igus products are also used in the manufacturing process itself!

igus’ line of Energy Chain cable carrier systems are used in a huge range of applications, including on manufacturing robots, like those in car-building plants. Energy Chains guide and protect cables and hoses that supply energy and other resources, without the risk of snagging on the many other moving parts in any busy plant. Triflex Energy Chain Systems allow for multi-axis movement – like the twisting motions of a robotic arm – without compromising cable protection.

igus’ line of linear products, known as DryLin, are also widely used in manufacturing plants. DryLin linear bearings and slides use the same self-lubricating properties of our iglide bearings, making them a reliable, clean solution. They will not attract dirt and dust, as they don’t require sticky lubricants, and unlike traditional ball bearing systems, any dirt and does that does find its way into the bearing will either be pushed aside by the sliding motion, or will meld into the plastic material without increasing the coefficient of friction.

Despite the wide range of applications and industries, the iglide car is still well received at all customer visits.

The iglide car crosses the border! Michigan to Ontario, Canada.2Customers are always so intrigued by how spacious the little car actually is. They are always surprised at how much legroom there is! 

The iglide car crosses the border! Michigan to Ontario, Canada.3

From Michigan, iglide on tour headed North to Detroit, and crossed the International Ambassador Bridge into Canada. The suspension bridge is privately owned by Grosse Point billionaire Manuel Moroun thorugh the Detroit International Bridge Company in United States, and the Canadian Transit Company in Canada. The bridge is the busiest international border crossing in North America in terms of trade volume. More than 25% of all merchandise trade between the US and Canada cross over this bridge.

The iglide car crosses the border! Michigan to Ontario, Canada.4 The iglide car crosses the border! Michigan to Ontario, Canada.5When the cars cross the bridge they cross over the Detroit River, they pass through two countries on one bridge. 

As the car crossed the border, the bridge’s border control was only concerned with one thing – how to enter a German license on their computer system! They loved the idea of the tour, and were curious about where the car was from, and where else it had been. They even took a car-shaped sticker to remind them to follow the blog as well!

The iglide car crosses the border! Michigan to Ontario, Canada.6

Once the car arrived in Canada for the second time along the tour, it was able to see a different side of Canada from the Yukon it explored early in the tour. Expecting to see bison, pronghorn, and mountains, the car instead saw miles of cornfields and dozens of wind turbines. The only animal to be seen was a muskrat!

In Canada, the car made more visits to customers, traveling with igus team members from both the USA and Canadian offices. With skilled staff memebers all over North America, the iglide tour has been like a bit of a family reunion!

The iglide car crosses the border! Michigan to Ontario, Canada.7

After a few more wonderful visits, it was time to travel back over the border to Detroit, where the iglide car spent the afternoon sightseeing.

The iglide car crosses the border! Michigan to Ontario, Canada.8

In Detroit, the car drove to the monument to boxer Joe Louis, known as “The Fist” in the middle of downtown. The statue is a memorial to the famous boxer, who is considered to be one of the greatest heavyweight boxers of all time. Commissioned by Sports Illustrated Magazine, it represents the power of Louis’ punch both in and out of the ring.

The iglide car crosses the border! Michigan to Ontario, Canada.9

After a long run of international travel, the iglide car headed south, towards Cleveland Ohio, where we met with members of the press who have been following the iglide tour since the beginning!

Look for us on the road,

Kayla